Is "StarterTRAK USB for MPC5643L" (TRK-USB-MPC5643L) compatible with TWR-MC-LV3PH low voltage motor control tower board?
Is is possible to run examples of motor control algorithms for MPC5643L with such setup ?
Where can I find code examples - if any ?
Best regards
Maciek
Hi Maciek,
I do not think it can be successfully done, as wrong PWM signals are connected to the interface and so 3-phase BLDC motor control is not possible.
Use either Kinetis or DSC based TWR board or if you want to use MPC5643L then look for example to http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/mpc5xxx-5x....
BR, Petr