Is StarterTRAK USB for MPC5643L compatible with TWR-MC-LV3PH ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is StarterTRAK USB for MPC5643L compatible with TWR-MC-LV3PH ?

745 Views
Maciek
Contributor V

Is "StarterTRAK USB for MPC5643L" (TRK-USB-MPC5643L) compatible with TWR-MC-LV3PH low voltage motor control tower board?

Is is possible to run examples of motor control algorithms for MPC5643L with such setup ?

Where can I find code examples - if any ?

 

Best regards

Maciek

Labels (1)
0 Kudos
Reply
1 Reply

603 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Maciek,

I do not think it can be successfully done, as wrong PWM signals are connected to the interface and so 3-phase BLDC motor control is not possible.

Use either Kinetis or DSC based TWR board or if you want to use MPC5643L then look for example to http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/mpc5xxx-5x....

BR, Petr

0 Kudos
Reply