Hello NXP community,
I have connected an external interrupt signal to PortX PinY on the MPC5744P.
I have enabled the interrupts by calling these functions.
I know that SIUL_EIRQ_24_31_IRQn is of type IRQn_Type. What are the names of the irq handler functions for SIUL_EIRQ which serve the interrupts of this type which might look something like this:
Would be good to have some documentation source for the same.
Thanks in advance,
KD
Hi,
you can install new ISR function and enable interrupt using below code
/* Install buttons ISR */
INT_SYS_InstallHandler(SIUL_EIRQ_24_31_IRQn, &buttonISR, NULL);
/* Enable buttons interrupt */
INT_SYS_EnableIRQ(SIUL_EIRQ_24_31_IRQn);
Anyway, vector table is defined in the startup_MPC5744P.s file, so you can refer to SDK's preinstalled IRQ handler function names.
BR, Petr