I want to use the BAM module of S32R274 and use uart to download the program.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I want to use the BAM module of S32R274 and use uart to download the program.

593 次查看
yinlei
Contributor III

I want to use the BAM module of S32R274 and use uart to download the program.How do I generate the corresponding RBL file, RBF file?

pastedImage_1.png

I found an example of 5748, but I don't know how 274 should generate these files.pastedImage_2.png

标记 (1)
0 项奖励
1 回复

530 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

as far as I know from the SW team they have support for S32R274 too, but this is not included in recent RAppID BL release. So please submit new Case in support system (https://community.nxp.com/docs/DOC-329745) so I can provide you a RBF file.

Thanks for understanding.

BR, Petr 

0 项奖励