Mpc5744p_fccu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mpc5744p_fccu

693 Views
fu860925
Contributor I

const fccu_config_ncf_t fccu1_NcfConfig2 =

{

    .functionID    = 2,

    .hwSwRecovery  = FCCU_NCF_HW_REC_FAULT,

    .reset         = FCCU_NCFS_NO_RESET,

    .timeoutEnable = false,

    .reactionType  = 0U,

    .callback      = NULL,

    .callbackParam = NULL

};

Fault 0-4, use the same config, two inject mothod,

FirstFCCU_DRV_SetNcfFake(0U,2U), no reaction, FCCU not switch to alarm or fault status, why?

 

SecondPMC->FIR = 0x1U;

When debug this line, s32 design studio show error, why?

Error : Error in ONCE status register during instruction execution.

Tags (1)
0 Kudos
Reply
1 Reply

593 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

This is and issue of SDK example code.

The FCCU works correctly if you configure it properly.

Please read my AN on how to work with FCCU:

https://www.nxp.com/docs/en/application-note/AN5284.pdf 

regards,

Peter

0 Kudos
Reply