How to use PE attach MPC5746C with JTag?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use PE attach MPC5746C with JTag?

886件の閲覧回数
dududdd
Contributor I

Hi,all

     S32 software prompted : "The target may have entered reset escalation. please power cycle the board."when I used PE attach MPC5746C with JTag. How can I solve this promblem?

     

     best regards!

     Thanks!

タグ(3)
0 件の賞賛
返信
2 返答(返信)

748件の閲覧回数
dududdd
Contributor I

When I tried to use LAUTERBACH to connect the board, it showed that debug port fail. And then,I pulled down the RESET PIN of the MPC5746C chip and pulled up the board.Meantimes,I used LAUTERBACH to connect the board. And then,I could debug it.

0 件の賞賛
返信

748件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

if you are able to connect using Lauterbach debugger, you should be also able to connect using PEMicro debugger. Which PEMicro debug probe you use and which version of S32DS you use?

Could you please send me the measurement of the reset signal after power on reset?

Regards,

Martin

0 件の賞賛
返信