hi,
Thanks One more clarification. As i understand CAN interface when compared to motherboard only one CAN Module (FlexCAN)is present and hence transferring between one can module to another is not possible right ? loop back needs to be done? please correct me if I'm wrong.
Regards,
Vignesh
Yes, you are right.
Theoretically you can do parallel connection of 2 FlexCAN modules, but connection to second module is almost impossible on this daughter card.
BR, Petr
And Does Same Apply to SPI because that also only one interface present in daughter board
yes.
Hi,
yes, both UART/eSCI and CAN interface are available on the MPC5777C daughtercard.
BR, Petr