Can UART/eSCI and CAN interface be tested with daughter board MPC5777c 516DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can UART/eSCI and CAN interface be tested with daughter board MPC5777c 516DS

645 Views
vignesh_v
Contributor III

Can UART/eSCI and CAN interface be tested with daughter board MPC5777c 516DS for basic functionality message transfer as im purchasing only daughter board right now?

Labels (1)
Tags (1)
0 Kudos
5 Replies

576 Views
vignesh_v
Contributor III

hi,

   Thanks One more clarification. As i understand CAN interface when compared to motherboard only one  CAN Module (FlexCAN)is present and hence transferring between one can module to another is not possible right ? loop back needs to be done? please correct me if I'm wrong.

Regards,

Vignesh 

0 Kudos

576 Views
PetrS
NXP TechSupport
NXP TechSupport

Yes, you are right.

Theoretically you can do parallel connection of 2 FlexCAN modules, but connection to second module is almost impossible on this daughter card.

BR, Petr

0 Kudos

576 Views
vignesh_v
Contributor III

And Does Same Apply to SPI because that also only one interface present in daughter board

0 Kudos

576 Views
PetrS
NXP TechSupport
NXP TechSupport

yes.

0 Kudos

576 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, both UART/eSCI and CAN interface are available on the MPC5777C daughtercard.

BR, Petr

0 Kudos