when i installed the CW11.1, i can't create a new project for MPC56X, because i can't find relevant device
Hi,
it was necessary to select "Qorivva" (this was a nickname for MPC5xxx devices in the past) during the installation:
To add support to existing installation, open Help -> Install New Software
and select:
Regards,
Lukas
Hi Lukas,
I am also using the chip MPC5602P and I have followed the instruction to update the Qorivva Support & MCU v11.1 Update for Qorivva. However, when I created a new project for MPC5602P, the component inspector is blank. I assume there is no SDK S32PA support for MPC5602P? I also tried S32 design studio power architecture, the component inspector is blank as well
Regards,
Joe
Hi,
yes, that's correct. There's no SDK for MPC56xx family of devices. We provided Autosar MCAL only:
https://www.nxp.com/design/automotive-software-and-tools/autosar:AUTOSAR-HOME
Regards,
Lukas
Hi Lukas,
Thank you for the reply. I installed the files
1. STUDIO_14.0.0_2013-02-26
2. MPC560XP_MCAL4.0_RTM_1.0.0_signed
3. MPC560XP_MCAL4.0_RTM_HF1_1.0.0_signed
For the MCAL4.0 RTM, I installed them under the path of "C:\EB\tresos\plugins"
When I clicked file -> import -> Existing Project into Workspace on Tresos studio, I selected "MPC560XP_MCAL4.0_RTM_1.0.0_Integration_Application" as root directory. (which then be copied into workspace). Then I clicked SampleApplication (PA, XPC560XP), it prompted a warning showing T2D11M10I0R0 is not installed. Where should I move all the files with T2D11M10I0R0 ending? So the Tresos Studio can load the configuration.
My intent here is to only configure the low level driver and pin configuration. no need for OS.
Best Regards,
Joe
Hi Joe,
I'm sorry for delayed response caused by Christmas holidays. This is for another team, so if it is still not resolved, please create new ticket here and it will be assigned to them:
Thanks,
Lukas
Hi
I operate according to your instructions, i meet a new issue below:
I disable the 1.0.3 version of buildtools, then it can continue again, but i don't know whether this will influence my developpment.
That should be ok, it's just older version which is not needed.
Regards,
Lukas
Hi,
if you really have SPC5604P34/SPC560P40, you are talking to wrong company. These are parts from ST. Please contact www.st.com
Regards,
Lukas