CMU with FCCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
672件の閲覧回数
mehmetkaradag
Contributor III

Hi, NXP engineers.

I am using MPC5777C.

i wanna get interrupt using FCCU if CMU_0_pll is damaged. Is there any aplication note or example about it. So which interrupt will code jump? FCCU or CMU?

mehmetkaradag_0-1684418058991.png

thanks for helps.

0 件の賞賛
返信
1 解決策
651件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Is there any application note or example about it.

No, as far as I know. It is simple settings of FCCU. For that I have AN here: Its the same module as for SPC5744P.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC574xP-FCCU-configuration-guide/ta-p/1105448

So which interrupt will code jump? FCCU or CMU?

Well, there is no interrupt for CMU in INTC module. So  only FCCU can trigger such interrupt based on signals from CMU.

petervlna_0-1684478705570.png

 

Best regards,

Peter

元の投稿で解決策を見る

1 返信
652件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Is there any application note or example about it.

No, as far as I know. It is simple settings of FCCU. For that I have AN here: Its the same module as for SPC5744P.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC574xP-FCCU-configuration-guide/ta-p/1105448

So which interrupt will code jump? FCCU or CMU?

Well, there is no interrupt for CMU in INTC module. So  only FCCU can trigger such interrupt based on signals from CMU.

petervlna_0-1684478705570.png

 

Best regards,

Peter