CMU with FCCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMU with FCCU

Jump to solution
648 Views
mehmetkaradag
Contributor III

Hi, NXP engineers.

I am using MPC5777C.

i wanna get interrupt using FCCU if CMU_0_pll is damaged. Is there any aplication note or example about it. So which interrupt will code jump? FCCU or CMU?

mehmetkaradag_0-1684418058991.png

thanks for helps.

0 Kudos
Reply
1 Solution
627 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Is there any application note or example about it.

No, as far as I know. It is simple settings of FCCU. For that I have AN here: Its the same module as for SPC5744P.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC574xP-FCCU-configuration-guide/ta-p/1105448

So which interrupt will code jump? FCCU or CMU?

Well, there is no interrupt for CMU in INTC module. So  only FCCU can trigger such interrupt based on signals from CMU.

petervlna_0-1684478705570.png

 

Best regards,

Peter

View solution in original post

1 Reply
628 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Is there any application note or example about it.

No, as far as I know. It is simple settings of FCCU. For that I have AN here: Its the same module as for SPC5744P.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC574xP-FCCU-configuration-guide/ta-p/1105448

So which interrupt will code jump? FCCU or CMU?

Well, there is no interrupt for CMU in INTC module. So  only FCCU can trigger such interrupt based on signals from CMU.

petervlna_0-1684478705570.png

 

Best regards,

Peter