********************************************************************************
* Detailed Description:
* Application performs basic initialization, setup PLL to maximum allowed freq.,
* setup clock for peripherals.
*
* This example shows, how to use ADC with ETimer to dim LED diode. Voltage on
* the output of the trimmer is converted to digital value which is used to
* control duty cycle of the PWM generated by ETimer.
*
* ------------------------------------------------------------------------------
* Test HW: MPC5775K-356DS, MPC57xx Motherboard
* MCU: PPC5775KMMY3A 0N76P
* Terminal:
* Fsys: PLL0 266MHz
* Z4 Core 133MHz
* Debugger: Lauterbach Trace32
* PeMicro USB-ML-PPCNEXUS
* Target: internal_FLASH (debug mode, release mode)
* EVB connection: UserLED1 connected to P19.4, connected jumper j53
*
*
*
********************************************************************************