Example MPC5775K ADC_example S32DS_1.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5775K ADC_example S32DS_1.0

Example MPC5775K ADC_example S32DS_1.0

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* setup clock for peripherals.

*

* This example shows, how to use ADC with ETimer to dim LED diode. Voltage on

* the output of the trimmer is converted to digital value which is used to

* control duty cycle of the PWM generated by ETimer.

*

* ------------------------------------------------------------------------------

* Test HW:         MPC5775K-356DS, MPC57xx Motherboard

* MCU:             PPC5775KMMY3A 0N76P

* Terminal:

* Fsys:            PLL0 266MHz

*                    Z4 Core 133MHz

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Target:          internal_FLASH (debug mode, release mode)

* EVB connection:  UserLED1 connected to P19.4, connected jumper j53

*

*

*

********************************************************************************

标签 (1)
附件
无评分
版本历史
最后更新:
‎03-21-2016 08:49 AM
更新人: