Dear all,
I have downloaded the demo "frdmmcxn947_lpi2c_interrupt_b2b_transfer_master" and it is function well that is using FLEXCOMM2 P4.0 and P4.1 as SDA and SCL pins.
I am going to set the i2c function to FLEXCOMM9 P2.4 and P2.3 by modifying the code in the demo code "frdmmcxn947_lpi2c_interrupt_b2b_transfer_master" as follows.
1) modify the code in "lpi2c_interrupt_b2b_transfer_master.c"
from
/* attach FRO 12M to FLEXCOMM2 */
CLOCK_SetClkDiv(kCLOCK_DivFlexcom2Clk, 1u);
CLOCK_AttachClk(kFRO12M_to_FLEXCOMM2);
to
/* attach FRO 12M to FLEXCOMM9 */
CLOCK_SetClkDiv(kCLOCK_DivFlexcom9Clk, 1u);
CLOCK_AttachClk(kFRO12M_to_FLEXCOMM9);
2) modify the code in "lpi2c_interrupt_b2b_transfer_master.c"
from
#define EXAMPLE_I2C_MASTER_BASE (LPI2C2_BASE)
to
#define EXAMPLE_I2C_MASTER_BASE (LPI2C9_BASE)
3) modify the code in "pin_mux.c"
void LPI2C2_InitPins(void)
{
/* Enables the clock for PORT2: Enables clock */
CLOCK_EnableClock(kCLOCK_Port2);
const port_pin_config_t port2_4_pinP1_config = {/* Internal pull-up resistor is enabled */
kPORT_PullUp,
/* Low internal pull resistor value is selected. */
kPORT_LowPullResistor,
/* Fast slew rate is configured */
kPORT_FastSlewRate,
/* Passive input filter is disabled */
kPORT_PassiveFilterDisable,
/* Open drain output is enabled */
kPORT_OpenDrainEnable,
/* Low drive strength is configured */
kPORT_LowDriveStrength,
/* Pin is configured as FC2_P0 */
kPORT_MuxAlt2,
/* Digital input enabled */
kPORT_InputBufferEnable,
/* Digital input is not inverted */
kPORT_InputNormal,
/* Pin Control Register fields [15:0] are not locked */
kPORT_UnlockRegister};
/* PORT2_4 (pin P1) is configured as FC2_P0 */
PORT_SetPinConfig(PORT2, 4U, &port2_4_pinP1_config);
const port_pin_config_t port2_3_pinP2_config = {/* Internal pull-up resistor is enabled */
kPORT_PullUp,
/* Low internal pull resistor value is selected. */
kPORT_LowPullResistor,
/* Fast slew rate is configured */
kPORT_FastSlewRate,
/* Passive input filter is disabled */
kPORT_PassiveFilterDisable,
/* Open drain output is enabled */
kPORT_OpenDrainEnable,
/* Low drive strength is configured */
kPORT_LowDriveStrength,
/* Pin is configured as FC2_P1 */
kPORT_MuxAlt2,
/* Digital input enabled */
kPORT_InputBufferEnable,
/* Digital input is not inverted */
kPORT_InputNormal,
/* Pin Control Register fields [15:0] are not locked */
kPORT_UnlockRegister};
/* PORT2_3 (pin P2) is configured as FC2_P1 */
PORT_SetPinConfig(PORT2, 3U, &port2_3_pinP2_config);
}
But the i2c cannot function.
Are there anything I am missing?
Please comment.
Thanks
Carl
Solved! Go to Solution.
Hi, @CarlLee
You're missing something, and you also need to change the macro definition clock rate. As follows:
#define LPI2C_MASTER_CLOCK_FREQUENCY CLOCK_GetLPFlexCommClkFreq(9u)
Clock selection is as follows:
Hope this helps you.
Best regards, Alex
Hi, @CarlLee
You're missing something, and you also need to change the macro definition clock rate. As follows:
#define LPI2C_MASTER_CLOCK_FREQUENCY CLOCK_GetLPFlexCommClkFreq(9u)
Clock selection is as follows:
Hope this helps you.
Best regards, Alex
Dear @Alex_Wang and @Alice_Yang,
Thanks for your help!
The solution is work properly.
I will add the i2c code to the face detection demo.
Previously I have successfully added i2c devices to the MCX_N9XX-BRK board with face detection.
This time, I need to transport the code to this new FRDM-MCXN947 board.
Regards,
Carl
Is there anyone who can give me some advice?
Hello @CarlLee
What about the signal when using logic analyzer measure?
How about using Config tool to config Flexcomm9, then refer to the code?
BR
Alice
Dear Alice, @Alice_Yang
I test the i2c at pins P2.4 and P2.3 as follow.
1) I start a new project by import SDK example "frdmmcxn947_lpi2c_interrupt_b2b_transfer_master".
2) I test the i2c function with another FRDM-MCXN947 which act as a i2c slave and function properly.
3) I am going to change the i2c master SDA and SCL pins to P2.4 and P2.3 respectively.
4) I use the Config tool to config Flexcomm9 pins SDA and SCL pins as P2.4 and P2.3 respectively.
5) I also activate the clock of Flexcomm9 in the Config tool.
6) I remark the line "LPI2C2_InitPins();" in the file "pin_mux.c"
7) I modify the line in red color "#define EXAMPLE_I2C_MASTER_BASE(LPI2C9_BASE)"
in the file "lpi2c_interrupt_b2b_transfer_master.c"
8 ) I remark two more lines in the file "lpi2c_interrupt_b2b_transfer_master.c" as below.
CLOCK_SetClkDiv(kCLOCK_DivFlexcom2Clk, 1u);
CLOCK_AttachClk(kFRO12M_to_FLEXCOMM2);
9) I build and download the code.
10) I attach the oscilloscope display below. The yellow line is SDA and the blue one is SCL.
The i2c is still not function.
Please advice.
Thanks,
Regards,
Carl
Hello @CarlLee
I haven't find the issue from your steps description.
Take a photo about hardware connection. Check whether connect the right pins.
If still can not work, please send your project to me, I help to check on my side. thanks.
BR
Alice
Dear @Alice_Yang,
After checking the code and the connection carefully, the i2c is fail to function.
The connection and the code are attached here.
Please advice,
Thanks,
Regards,
Carl