Hi,
I installed the latest (v3.1) MCUXpresso Secure Provisioning Tool on a PC running on Windows 11 Pro Insider Preview (OS build - 22509.1011). The tool installed successfully but I can't use it afterwards.
I keeps on crashing with the following message:
Any help would be much appreciated. Thank in advance.
已解决! 转到解答。
Hi,
BTW, there was issue on Windows with some combination of locale settings. You can give it a chance on Windows 11 if you switch to English US region. But take it as a blind try.
Regards,
Libor
Jeff,
SEC tool v4 is already available. Is your feedback related to v3.1 or v4?
If this is problem in v4, can you be more specific, what exactly means "Change to support Unicode UTF-8"?
Thank you for the feedback.
Hi Pedro and kanimozhi_t,
Thank you for your inputs. We're sorry for inconvenience with problem with region settings, this problem can be reproduced also on Win10 and will be fixed in v4. Thank you for providing details how to reproduce it
Hi,
BTW, there was issue on Windows with some combination of locale settings. You can give it a chance on Windows 11 if you switch to English US region. But take it as a blind try.
Regards,
Libor
Hi kanimozhi_t,
SEC tool was not tested on Windows 11 yet, so currently we do not have any information, whether it will work. Supported operating systems are listed in the Release notes.
About un-installation: the default uninstaller does not touch the data, created by the tool (e.g. workspaces) and also preferences. The preferences are located in <user home>\.nxp\secure_provisioning_v<version>\. The preferences are backward compatible, so for example SEC Tool v3 can load preferences from SEC Tool v2, if preferences for v3 does not exist yet.
Hope this helps,
Basically we earlier used,
And the tool didn't work. So I changed as follows,
Now the tool is working as intended and it would be nicer to have the India region (or UK for that matter) supported.