I get the following error from the uuu tool when running on ubuntu 18.1 under vmware, the same lst file works fine from windows, I know this is an issue with vmware but just looking for any insight on how to resolve this issue.
Wait for Known USB Device Appear...
New USB Device Attached at 1:1
1:1>Start Cmd:SDP: boot -f imx-boot-imx8mmlfbr-mfgtool.bin
6400%1:1>Okay
New USB Device Attached at 1:1
1:1>Start Cmd:SDPV: delay 1000
1:1>Okay
1:1>Start Cmd:SDPV: write -f imx-boot-imx8mmlfbr-mfgtool.bin -skipspl
100%1:1>Okay
1:1>Start Cmd:SDPV: jump
6400%1:1>Okay
New USB Device Attached at 1:3
1:3>Start Cmd:FB: ucmd setenv fastboot_dev mmc
1:3>Fail Bulk(W):LIBUSB_ERROR_TIMEOUT
Thanks,
Tom
Hi Tom,
Have you also tried running UUU from a Ubuntu 18 native machine in order to discard that the issue is caused by the virtual machine environment?
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------