Amazon-FreeRTOS unavailable in SDK v2.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Amazon-FreeRTOS unavailable in SDK v2.6

1,113 次查看
stefanlindblad
Contributor I

sdk 2.6.0 free_rtos

Hi

Requested and built SDK v2.6 WITH Amazon-FreeRTOS for MKL1x.

Same SDK is used both for MKL1x and MKL2x but FreeRTOS is only available when creating projects for KL2x.

Will it be reenabled in next update or should I stick with v2.5, where it is available?

Regards, Stefan

标记 (2)
0 项奖励
回复
1 回复

1,027 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Dear Stefan,

You're right, there's a little problem with the SDK from the KL1x, but if you import the SDK from the KL1x a FRDM-KL43 that can be used to develop your project.

pastedImage_1.png

If you do this you can select the FreeRTOS option. You will only need to adjust the memory location according to the MCU version are you using.

pastedImage_2.png

I hope this helps you.

Best Regards,

Alexis Andalon