When I build the SDK 2.4 for MK26 device, the only driver present is "fsl_clock". The rest of the drivers are missing.
Drivers are available for the MK65 and MK66 but not MK26
Hi Roberto, geoff_s and Nick
We are going to have a new deployment this week. thank you all.
Regards
Daniel
I also ran into this problem with SDK for the TWR-K22F120M.
After testing a few variations, I discovered it was only an issue if I attempted to generate a project with the wizard and selected ANY of the CMSIS drivers. The CMSIS drivers have header file includes for the non-CMSIS drivers, but the non-CMSIS files are not automatically added to the project. If you select the CMSIS driver AND the associated non-CMSIS driver, all is well. Other than that, all the example projects and any custom project variations (that I tried) compile without modification.
Same issue occurs with KL17Z.
Thanks, I will report this issue to software team
Regards
Daniel
The same problem exists for the MKL27Z4, the archive only contains fsl_clock under devices/MKL27Z4/drivers but no other files.
btw, why is there an MKL43Z4 folder at all, if I 'build' the sdk for the MKL27Z4? of course they are similar and AFAIK the suggested dev board for the kl27z is the frdm-kl43z but then an option 'support recommended dev kit' would make sense...
Thank you
Regards
Daniel
Hi Roberto:
Thank you for reporting this issue, I will check it with software team and get it back to you.
Regards
Daniel