Hello all,
When using the MCUXpresso SDK 2.5 with arm embedded GCC compiler I believe there is a bug in the LPC54606 linker file.
The following memory areas are declared:
/* Specify the memory areas */
MEMORY
{
m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400
m_text (RX) : ORIGIN = 0x00000400, LENGTH = 0x0007FC00
m_data (RW) : ORIGIN = 0x20000000, LENGTH = 0x00028000
m_sramx (RW) : ORIGIN = 0x04000000, LENGTH = 0x00008000
m_usb_sram (RW) : ORIGIN = 0x40100000, LENGTH = 0x00002000
}
But there is a mapping to the memory area "m_data_3" that does not exist:
/* Initializes stack on the end of block */
__StackTop = ORIGIN(m_data_3) + LENGTH(m_data_3);
__StackLimit = __StackTop - STACK_SIZE;
PROVIDE(__stack = __StackTop);
This results in the following GCC linker warning:
LPC54606J512_flash.ld:183: warning: memory region `m_data_3' not declared
The code does not work since the stack is now undefined. As workaround I use the LPC54608J512 linker file which works but it is not the best solution.
已解决! 转到解答。
Hi Jelle,
This defect will be fixed in next release.
Thank you for bringing the problem to our attention.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Jelle,
This defect will be fixed in next release.
Thank you for bringing the problem to our attention.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------