LPC54102 USART Driver - TX Ring Buffer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54102 USART Driver - TX Ring Buffer

612 Views
BTaylor
Contributor III

Does the latest mcuxpresso SDK for LPC54102 provide TX ring buffer support? The version that I am currently using - 2.6.1 - only provides ring buffer support for RX. This seems to me to be a significant deficiency, especially considering that RX ring buffer support was provided in the 'old' LPCOpen SDK. 

If such support is truly not yet provided in the mcuxpresso SDK, are there plans to add such support in the (hopefully near) future? 

Before I start building a new USART driver...has someone on this forum perhaps already extended the mcuxpresso to add TX ring buffer support?

Tags (3)
0 Kudos
Reply
1 Reply

531 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Currently, the SDK version forLPCXpresso54012 is V2.6.1, I do not think that the version has added the TX buffer ring, only RX buffer ring has implemented.

Hope it is helpful

BR

XiangJun Rong

xiangjun_rong_0-1695009401286.png

 

0 Kudos
Reply