KW41Z With SDK2.2.3 HardFault

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KW41Z With SDK2.2.3 HardFault

1,156 次查看
agalliazzo
Contributor I

Dear sirs,

While trying to use the SDK example frdmkw41z_wireless_examples_thread_end_device_freertos (but it happen also with router eligible thread end device) I can join the device to the thread network created with Openthread but every time I try to send something pushing a button the KW41Z enter in an hard fault condition.

Querying the board though serial port works.

I'm not able to debug the Hardfault cause it point to strange stack position.

Does anyone have some advice?

Best

Alessio

标记 (2)
0 项奖励
回复
3 回复数

1,145 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

 

Do you just use the example without any modification ?

 

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,138 次查看
agalliazzo
Contributor I

Hi, yes, it's a brand new demo project. No edit in the files. The network leader is an OpenThread based border router with a nrf52840 RCP.

With other development board from Nordic the network works without issues.

Best

0 项奖励
回复

1,128 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

I test on two frdm-kw41. It woks well. So may be the kw41 has compatibility with other company's product. I do not have the Nordic product. I also can't test this problem.

0 项奖励
回复