KW41Z With SDK2.2.3 HardFault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW41Z With SDK2.2.3 HardFault

1,754件の閲覧回数
agalliazzo
Contributor I

Dear sirs,

While trying to use the SDK example frdmkw41z_wireless_examples_thread_end_device_freertos (but it happen also with router eligible thread end device) I can join the device to the thread network created with Openthread but every time I try to send something pushing a button the KW41Z enter in an hard fault condition.

Querying the board though serial port works.

I'm not able to debug the Hardfault cause it point to strange stack position.

Does anyone have some advice?

Best

Alessio

タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,743件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

 

Do you just use the example without any modification ?

 

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,736件の閲覧回数
agalliazzo
Contributor I

Hi, yes, it's a brand new demo project. No edit in the files. The network leader is an OpenThread based border router with a nrf52840 RCP.

With other development board from Nordic the network works without issues.

Best

0 件の賞賛
返信

1,726件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

I test on two frdm-kw41. It woks well. So may be the kw41 has compatibility with other company's product. I do not have the Nordic product. I also can't test this problem.

0 件の賞賛
返信