I seem to have no end of trouble trying to get projects and repositories structured and named like I want. I'm hoping someone can set me straight on what exactly I'm doing wrong.
My general organization structure is that I have each project in its own folder:
s:\projects\someproject
s:\projects\anotherproject
These top-level project folders are not the MCUX projects - they include everything for the project, including non-code stuff like marketing materials, user manuals, CAD/CAM files, and so on. These go into standardized folders, like \cad, \eda, and (most importantly for this discussion) \code.
The problem I'm having right now is that the Git Repositories view shows the folder name and not the repository name - so every project that complies with this layout shows up as code [master]. I can rename the branch but not the repository.
Am I doing something wrong? Is it really that unusual to have a folder name that doesn't match the project name? Is there any way to fix this?
Thanks,
Scott
Hi Scott,
after thinking more about it, I think I see what you mean (like in my screenshot with using 'git' as label as I have named my folders 'git' too. So in your case it would show up as 'code' as you have the repository in there.
I don't think there is an easy way around it, except you would name your folders differently of course.
Erich
Hi Scott,
could you share a screenshot showing what you mean?
The project explorer view shows the project name which does not have to be the same as the folder name, plus the git repository and branch. See below the relationships:
The git repositories view shows the git repos as they are on disk, with the name of the folder, as shown below:
I hope this helps,
Erich
It's really the Git Repositories view I'm concerned with:
All of my projects are going to end up being called 'code' in this view when I'm done organizing them. I can still tell which project is which based on the location, it's just kind of an annoying quirk.
Scott