No compatible probes available for LPCXpresso804

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No compatible probes available for LPCXpresso804

Jump to solution
1,076 Views
witaradya
Contributor II

 

Hi, everyone

I have installed MCUXpressoIDE v11.6.0 onto win10 and then install SDK_2.x_LPCXpresso804 version 2.12.0.

witaradya_3-1658902717477.png

 

I also import the examples(install together with SDK), and then I tried to build lpcxpresso804_led_blinky project, no error and warning appear. Then I debug it, when I debug the problem happened like this :

witaradya_0-1658898027607.pngwitaradya_1-1658898082960.png

witaradya_2-1658902647985.png

 

Anyone can help me to solve this problem?
Thank you.

 

0 Kudos
Reply
1 Solution
1,056 Views
witaradya
Contributor II

Solved. 

I try to restart my PC and then open the IDE, build, and debug. The error nor appear and can detect the dev board.

Thank you.

View solution in original post

0 Kudos
Reply
4 Replies
1,057 Views
witaradya
Contributor II

Solved. 

I try to restart my PC and then open the IDE, build, and debug. The error nor appear and can detect the dev board.

Thank you.

0 Kudos
Reply
1,065 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

I guess you haven't install driver.

Please download and install debug driver below

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=LPC11Uxx-Debug-Probe-VCOM

Best Regards

Jun Zhang

 

0 Kudos
Reply
1,063 Views
witaradya
Contributor II

Thank you,

I use Win10, so the driver automatically installed. I have tried to update the driver, but the error keep appear.

But when I am using IAR, there is no error to download and debug program.

 

Best regards,

Witaradya

0 Kudos
Reply
1,057 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

To identify if the problem is caused by old associations, Please create a NEW workspace and import a SDK demo. Try again.

Thanks,

Jun Zhang

0 Kudos
Reply