Dear all,
I'm developing a project for microcontroller K20 using MCUXpresso IDE v11.0.0 [Build 2516] [2019-06-05].
I did the pin configuration using Pins section and I saved it.
I have this problem: when I close and open the project, the MCUXpresso doesn't load the pin configuratin and I have to repeat it evrey time.
Does someone know how can I configure the MCUXpresso to load the pin configuration?
Many thanks in advance for your support.
Kind Regards
Solved! Go to Solution.
Hello,
I solved the problem. There were two *.mix files in the workspace.
Thank you to all.
Kind Regards,
Stefano
Hello,
I solved the problem. There were two *.mix files in the workspace.
Thank you to all.
Kind Regards,
Stefano
Hi,
Thank you for your input.
Have a nice day!
Regards
Soledad
Hi,
Pins tool configuration is loaded automatically. Be careful if you have several projects in the workspace - Pins tool can open just one configuration. If you modify Pins configuration, hit [Update Code] button to save configuration and apply changes into source code.
Regards
Marek
Hello,
by Pins section you mean Pins tool probably. Is <projectname>.mex file created in the project? Is there just one *.mex file inside? Would be good if you can attach the mex here.
BTW - are you aware that there's IDE 11.1.0?
Regards,
Libor