MCUXpresso IDE doesn't keep the pin configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE doesn't keep the pin configuration

Jump to solution
1,458 Views
chobin
Contributor III

Dear all,

I'm developing a project for microcontroller K20 using MCUXpresso IDE v11.0.0 [Build 2516] [2019-06-05].

I did the pin configuration using Pins section and I saved it.

I have this problem: when I close and open the project, the MCUXpresso doesn't load the pin configuratin and I have to repeat it evrey time.

Does someone know how can I configure the MCUXpresso to load the pin configuration?

Many thanks in advance for your support.

Kind Regards

0 Kudos
1 Solution
1,394 Views
chobin
Contributor III

Hello,

I solved the problem. There were two *.mix files in the workspace.

Thank you to all.

Kind Regards,

Stefano

View solution in original post

0 Kudos
4 Replies
1,395 Views
chobin
Contributor III

Hello,

I solved the problem. There were two *.mix files in the workspace.

Thank you to all.

Kind Regards,

Stefano

0 Kudos
1,394 Views
soledad
NXP Employee
NXP Employee

Hi,

Thank you for your input.

Have a nice day!

Regards

Soledad

0 Kudos
1,394 Views
marek-trmac
NXP Employee
NXP Employee

Hi,

Pins tool configuration is loaded automatically. Be careful if you have several projects in the workspace - Pins tool can open just one configuration. If you modify Pins configuration, hit [Update Code] button to save configuration and apply changes into source code.

Regards

Marek

Regards,
Marek
0 Kudos
1,394 Views
liborukropec
NXP Employee
NXP Employee

Hello,

by Pins section you mean Pins tool probably. Is <projectname>.mex file created in the project? Is there just one *.mex file inside? Would be good if you can attach the mex here.

BTW - are you aware that there's IDE 11.1.0?

Regards,

Libor

0 Kudos