Dear all,
I'm developing a project for microcontroller K20 using MCUXpresso IDE v11.0.0 [Build 2516] [2019-06-05].
I did the pin configuration using Pins section and I saved it.
I have this problem: when I close and open the project, the MCUXpresso doesn't load the pin configuratin and I have to repeat it evrey time.
Does someone know how can I configure the MCUXpresso to load the pin configuration?
Many thanks in advance for your support.
Kind Regards
已解决! 转到解答。
Hi,
Pins tool configuration is loaded automatically. Be careful if you have several projects in the workspace - Pins tool can open just one configuration. If you modify Pins configuration, hit [Update Code] button to save configuration and apply changes into source code.
Regards
Marek
Hello,
by Pins section you mean Pins tool probably. Is <projectname>.mex file created in the project? Is there just one *.mex file inside? Would be good if you can attach the mex here.
BTW - are you aware that there's IDE 11.1.0?
Regards,
Libor