MCUXpresso IDE 11.1.0 Breakpoint error message

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso IDE 11.1.0 Breakpoint error message

1,098件の閲覧回数
HeMyFAE
NXP Employee
NXP Employee

 Dear TEch support,

While debuging a problem  I tried to set a breakpoint and got the following error message below:

"Breakpoint installation  failed : Unmatched quote" .

It prevents me from setting a breakpoint.

What does that means?

Regards,

hy

pastedImage_1.png

0 件の賞賛
3 返答(返信)

1,024件の閲覧回数
converse
Senior Contributor V

The last time this was reported it was because there was a strange character in the full directory path of the file. Breakpoints are set using the full path, so check the name. If there is a problem in the name, you’ll need to change it.

0 件の賞賛

1,024件の閲覧回数
HeMyFAE
NXP Employee
NXP Employee

The customer was copy a project from one PC to another.

Perhaps the project was not export and imported properly so the files's directory was not align properly, right?

Can you reference a blog of the reported issue?

where in the project setting is this directory path that you have to change?

0 件の賞賛

1,024件の閲覧回数
converse
Senior Contributor V

I refer to the location, on the disk, of the file. This is probably also the location of the workspace.

the question I was referring to was thiis

https://community.nxp.com/thread/532550 

if the project was Exported and Importes, there should be no problem. However if the directory name contains strange characters then this can cause the problem you are reporting.

0 件の賞賛