MCUXpresso ERROR:StubMonSemihost

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso ERROR:StubMonSemihost

902 次查看
Yuan1
Contributor I
Everything went well when I compiled the program in GUI GUIDER, but after importing the file into MCUXpresso, the following problems were displayed when debugging Error in final launch sequence: Failed to execute MI command: StubMonSemihost: -interpreter-exec console "mon semihost enable"Error message from debugger back end: "monitor" command not supported by this target. Failed to execute MI command: StubMonSemihost: -interpreter-exec console "mon semihost enable"Error message from debugger back end: "monitor" command not supported by this target. "monitor" command not supported by this target. I try change its SDK Debug console,and re-install mcuxpresso. by a pity College Students
0 项奖励
回复
2 回复数

890 次查看
Yuan1
Contributor I

sorry for the typesetting,here is the new one

Everything went well when I compiled the program in GUI GUIDER, but after importing the file into MCUXpresso, the following problems were displayed when debugging

Error in final launch sequence: Failed to execute MI command: StubMonSemihost: -interpreter-exec console "mon semihost enable"Error message from debugger back end: "monitor" command not supported by this target. Failed to execute MI command: StubMonSemihost: -interpreter-exec console "mon semihost enable"Error message from debugger back end: "monitor" command not supported by this target. "monitor" command not supported by this target.

I try change its SDK Debug console,and re-install mcuxpresso.

by a pity College Students

0 项奖励
回复

886 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Please attach the logs (Help => MCUXpresso IDE Save Info for Support)...

Regards,
MCUXpresso IDE Support

0 项奖励
回复