MCUXpresso ERROR:StubMonSemihost

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso ERROR:StubMonSemihost

900 Views
Yuan1
Contributor I
Everything went well when I compiled the program in GUI GUIDER, but after importing the file into MCUXpresso, the following problems were displayed when debugging Error in final launch sequence: Failed to execute MI command: StubMonSemihost: -interpreter-exec console "mon semihost enable"Error message from debugger back end: "monitor" command not supported by this target. Failed to execute MI command: StubMonSemihost: -interpreter-exec console "mon semihost enable"Error message from debugger back end: "monitor" command not supported by this target. "monitor" command not supported by this target. I try change its SDK Debug console,and re-install mcuxpresso. by a pity College Students
0 Kudos
Reply
2 Replies

888 Views
Yuan1
Contributor I

sorry for the typesetting,here is the new one

Everything went well when I compiled the program in GUI GUIDER, but after importing the file into MCUXpresso, the following problems were displayed when debugging

Error in final launch sequence: Failed to execute MI command: StubMonSemihost: -interpreter-exec console "mon semihost enable"Error message from debugger back end: "monitor" command not supported by this target. Failed to execute MI command: StubMonSemihost: -interpreter-exec console "mon semihost enable"Error message from debugger back end: "monitor" command not supported by this target. "monitor" command not supported by this target.

I try change its SDK Debug console,and re-install mcuxpresso.

by a pity College Students

0 Kudos
Reply

884 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Please attach the logs (Help => MCUXpresso IDE Save Info for Support)...

Regards,
MCUXpresso IDE Support

0 Kudos
Reply