I have the UM11035 Dev board with the LPC54608 MCU. I used LPCScrypt to put the J-Link debugging firmware on the on board debugger. I am able to use JFlashLite.exe to download binaries. But I can't seem to be able to start a debug session through MCUExpresso with the J-Link.
I set up GDB Segger Interface Debugging configuration for USB with SWD to use the generated .axf file.
I get an error: "Error in final launch sequence Cannot get Jtag device". The debug configuration is set up to do SWD.
Question:
1) Can this be done?
2) Does the J-Link firmware support semi-hosting?
3) Can I use the dev board with J-Link for the SEGGER SystemView?
已解决! 转到解答。
It sounds like you are trying to manually set up your launch configuration - this is not what you would normally do using MCUXpresso IDE. Instead you should let the IDE detect your probe, then auto-generate the appropriate launch configuration. The simplest way to do this is to start your debug session using the "Debug" button inside the Quickstart Panel.
I would suggest looking at the following sections of the MCUXpresso IDE v10.0.2 User Guide for more information...
Chapter 3 - Debug Solutions Overview
Chapter 9 - Debugging a Project
Regards,
MCUXpresso IDE Support
It sounds like you are trying to manually set up your launch configuration - this is not what you would normally do using MCUXpresso IDE. Instead you should let the IDE detect your probe, then auto-generate the appropriate launch configuration. The simplest way to do this is to start your debug session using the "Debug" button inside the Quickstart Panel.
I would suggest looking at the following sections of the MCUXpresso IDE v10.0.2 User Guide for more information...
Chapter 3 - Debug Solutions Overview
Chapter 9 - Debugging a Project
Regards,
MCUXpresso IDE Support