Installed SDK micro not showing at the SDK wizard

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Installed SDK micro not showing at the SDK wizard

跳至解决方案
706 次查看
fernando_casado
Contributor II

I have run the installation program for MCUXpresso version 11.2.1 as administrator.

I have launched the MCUXpresso with administrator privileges.

I got the next messages in the log:

fernando_casado_2-1696935136353.png

I have gone to the "Install New Plugin SDK" window, and I have installed the package for micro LCP54606J256. Once the installation finishes, it says that micro is installed

fernando_casado_0-1696934823443.png

But when I go to the Installed SDKs view, nothing appears.

fernando_casado_1-1696934931576.pngThe log shows the next errors:

fernando_casado_3-1696936751600.png

I have pressed the "Recreate and reload part support info" button, but nothing happens.

I have restarted the MCUXpresso (again as administrator) but nothing happens.

I have repeated the process for microcontroll LPC5502 with similar results: nothing shown in the Installed SDKs view.

 

Any help?

 

Regards

 

Fernando

0 项奖励
回复
1 解答
676 次查看
RaRo
NXP TechSupport
NXP TechSupport

Hello @fernando_casado,

If possible, could you please change to the newest MCUXpresso IDE v11.8.0?

Is the same issue happening there?

Best regards, Raul.

在原帖中查看解决方案

2 回复数
660 次查看
fernando_casado
Contributor II

Yes, after getting crazy for two days, on Wednesday I updated to the latest MCUXpresso version and the problem disappeared. It seems it is a bug related to version  11.2.1

Regards

Fernando

677 次查看
RaRo
NXP TechSupport
NXP TechSupport

Hello @fernando_casado,

If possible, could you please change to the newest MCUXpresso IDE v11.8.0?

Is the same issue happening there?

Best regards, Raul.