Hi there,
I work with the CLRC663 chip and read IO15693 transponders.
When I call the function phalI15693_ReadMultipleBlocks () everything works as described.
The bytes: SOF 20 23 [UID] FBN NOB CRC CRC EOF are sent via RFID.
But now I need an individual command in the following form:
SOF 20 AB 02 [UID]
AB is the command and 02 is a constant. How can I configure such individual commands?
Many thanks for your help
Hi @mark2030 ,
The API of "phpalSli15693_Exchange" can be used for that purpose. Please kindly refer to phpalSli15693.c for more details.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------