How to get the Installed SDK view?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get the Installed SDK view?

998 Views
sanketkulkarni
Contributor III

I am using LPC Xpresso for Rapid Iot board. But  I am not getting the option of installed sdk in show view. 

How can I get the "Installed SDK" view. I tried to find it in: "Windows -> Show Views -> Others -> " but it is not present in this show view option. Can you guide me on this, any shortcuts or other way to get the Installed SDK view.

Tags (1)
0 Kudos
Reply
2 Replies

885 Views
BlackNight
NXP Employee
NXP Employee

Your screenshot indicates that you are using LPCXpresso, and not MCUXpresso.

You should use the MCUXpresso IDE (you can get it from http://www.nxp.com/mcuxpresso/ide).

I hope this helps,

Erich

0 Kudos
Reply

885 Views
sanketkulkarni
Contributor III

Yes. I was using Xpresso. I did not notice MCU Xpresso is different. Thank you.

   Sir, I would like to ask for one more help if possible, I am working on Rapid IoT Prototyping kit for Hackster Competition. I have participated in this to see if I can develope a full fledge product out of it within the two months time. 

   Sir, I would like to ask about any resources by which I can minimise error while doing project and develope the firmware fast and efficiently. Any reading material which can guide me to avoid mistakes. Reading material which will help me develope firmware. 

   For now I am refering the SDK and User manual documentation.

0 Kudos
Reply