MCUXpresso KL26Z JlinkOPenSDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso KL26Z JlinkOPenSDA

573 Views
HeMyFAE
NXP Employee
NXP Employee

Dear Tech support,

I tried to upgrade the debugging firmware from OPENSDA CDC to Jlink Open SDA .

I hold down SW2 and plug in the USB cable on J10/SDA port.

The PC see the the bootloader. 

I  tried all 3 different versions generic and one specific to KL26Z.

The files seems to upload just fine, but after unplugging and re-plugging the usb cable the PC/Teraterm/Device manager cannot find the Jlink debugger.

The debugger light does not blink either.

I need to change from OpenSDA-CDC to Jlink because MCUXpresso won't recognize OpenSDA-CDC. 

Regards,

hy

I tried to upgrade the pastedImage_2.pngOPenSDA firmware with pastedImage_1.png

0 Kudos
1 Reply

488 Views
BlackNight
NXP Employee
NXP Employee

Are you using Windows 10? Then you have to stop the storage service first, see Recovering OpenSDA Boards with Windows 10 | MCU on Eclipse 

I hope this helps,

Erich

0 Kudos