Hello World and Blinky Demo Apps won't Prog/Debug in Xpresso IDE v11.1.1, But Work Fine in Xpresso IDE v11.0.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hello World and Blinky Demo Apps won't Prog/Debug in Xpresso IDE v11.1.1, But Work Fine in Xpresso IDE v11.0.1

1,167件の閲覧回数
gregs5451
Contributor III

I'm using the unmodified demo apps for the FRDM-KE02Z40M board.

Errors:

pastedImage_1.png

Debugger Console tab:

monitor selectcore 0

"monitor" command not supported by this target.

continue

The program is not being run.

 

Console tab:

P&E Semihosting Console

Connection closed by the GDB server.

 

<Device is being erased and programmed and runs OK standalone, but will not run from debugger connection.>

UPDATE CORRECTION: Device is NOT getting erased OR programmed with Xpresso IDE v11.1.1.

Console info:

     IDE v11.0.1.                                                                        IDE v11.1.1.

pastedImage_2.png

What's the problem?

0 件の賞賛
返信
2 返答(返信)

1,025件の閲覧回数
gregs5451
Contributor III

Hi Luis,

I have contacted PEmicro support. Based upon the information I sent them, they confirmed that there seems to be a problem (drivers maybe?), although they could not confirm with my specific FRDM board.

They requested more specific information which I just sent.

Stay tuned and I will post results if successful.

Gregg

0 件の賞賛
返信

1,025件の閲覧回数
Heron
Contributor II

This is the same problem that I have already posted as "GDB server closes connection" by Luis Espinal Mar 19, 2020

0 件の賞賛
返信