Hi team,
I was trying to create a new project in MCUxpresso IDE (instead of importing the SDK example project).
I have followed the steps mentioned in the section "5.1 New Project Wizard" of the MCUxpresso IDE user guide document. But when i am trying to debug using the existing USB cable or even using the PEmicro debugger, the below mentioned error i am facing when i click on debug icon in IDE.
I am also attaching the user guide for reference, Kindly suggest any configuration or settings in the IDE to solve the above error which is not seen when using the existing SDK examples.
Hi @Jeevan ,
Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.
Your log mentioned the flashdriver have issues.
So, you need to check your new created project flashdriver for the CMSIS DAP:
Please check it, you also can compare it with the SDK demo which is working.
Wish it helps you!
If you still have question about it, please kindly let me know.
Best Regards,
Kerry
Hi @Jeevan ,
In fact, if you don't use the CMSIS driver operation, you tottaly can don't use it.
But, if you still have issue, you can refer to the working SDK demo, to add the related CMSIS Driver.
Best Regards,
Kerry
HI @Jeevan ,
You can refer to my document:
chapter 3. SAI MCUXpresso project creation,
It is also the new project creation, you can try that method.
If you still have question about it, please kindly let me know.
Best Regards,
Kerry