Debian 10 has been released over the weekend. During installation several missing dependencies are reported. All except one I could resolve. The remaining one is libwebkitgtk-1.0-0. This is no longer available through APT. Is there a workaround/solution?
Verifying archive integrity... All good. Uncompressing mcuxpressoide installer 100% Installing... (Reading database ... 160674 files and directories currently installed.) Preparing to unpack JLink_Linux_x86_64.deb ... Removing /opt/SEGGER/JLink ... Unpacking jlink (6.449) over (6.449) ... Setting up jlink (6.449) ... Selecting previously unselected package mcuxpressoide. (Reading database ... 160674 files and directories currently installed.) Preparing to unpack mcuxpressoide-11.0.0_2516.x86_64.deb ... Unpacking mcuxpressoide (11.0.0) ... dpkg: mcuxpressoide: dependency problems, but configuring anyway as you requested: mcuxpressoide depends on libncurses5:i386. mcuxpressoide depends on libwebkitgtk-1.0-0; however: Package libwebkitgtk-1.0-0 is not installed.
let me paste over
I think this might be late since I was using Ubuntu 18.04 until recently when I upgraded to latest version 19.04
Tried to install Mcuxpresso IDE I encountered some dependency errors but managed to solved it. I had already replied to question about it but decided #to write main post about it.
This is what I did (installed the dependencies)
(my laptop is 64 bit)
sudo apt install libusb-1.0-0-dev
sudo apt install dfu-util
download amd64 build of icu 60.1-1
install the package (open terminal from the file location)
sudo dpkg -i libicu60_60.1-1ubuntu2_amd64.deb
download libjavascriptcoregtk-1.0-0_2.4.11-4
and install
sudo dpkg -i libjavascriptcoregtk-1.0-0_2.4.11-4_amd64.deb
download libwebkitgtk-1.0-0_2.4.11-4
and install
sudo dpkg -i libwebkitgIDEIDEtk-1.0-0_2.4.11-4_amd64.deb
install IDE(open terminal from file location)
install.....
sudo chmod +x ./mcuxpressoide-11.0.0_2516.x86_64.deb.bin
sudo ./mcuxpressoide-11.0.0_2516.x86_64.deb.bin
After this you should home and dry :smileycool:
Everything worked well.
If you have any problem you can reply to this post.
Hi,
1.Problem: Installing mcuexpresso 11.4.1 (mandatory requirement) on Ubuntu 24.04
2.Error: package description
mcuxpressoide depends on libncurses5; however:
Package libncurses5 is not installed.
mcuxpressoide depends on libusb-1.0-0-dev; however:
Package libusb-1.0-0-dev is not installed.
mcuxpressoide depends on dfu-util; however:
Package dfu-util is not installed.
mcuxpressoide depends on libwebkit2gtk-4.0-37; however:
Package libwebkit2gtk-4.0-37 is not installed.
3. Partial solution for all packages excerpt libwebkit2gtk-4.0-37
Package libwebkit2gtk-4.0-37 is not available, but is referred to by another package. This may mean that the package is missing, has been obsoleted, or is only available from another source
Does NXp have a solution for this case ???
*Update*
This link solve this:
https://github.com/bambulab/BambuStudio/issues/3973
Just remember to restore back:
/etc/apt/sources.list.d/ubuntu.sources
with the original one after mcuexpresso launches
Anyway NXP should provide a solution imho
Regards
Sbm
Alexis, Bonny seems to have a solution by manually installing the obsolete packages. Is NXP planning to remove these dependencies to obsolete packages in one of the upcoming releases? More and more distributions seem to have issues with this (Ubuntu 19.04, Debian 10)...
Hi Alexis,
No, this package is also not available:
$ sudo apt update Hit:1 http://ftp.be.debian.org/debian buster InRelease Get:2 http://ftp.be.debian.org/debian buster-updates InRelease [46.8 kB] Hit:3 http://security.debian.org/debian-security buster/updates InRelease Fetched 46.8 kB in 0s (133 kB/s) Reading package lists... Done Building dependency tree Reading state information... Done All packages are up to date.
$ sudo apt-get install -y libwebkitgtk-3.0-0 Reading package lists... Done Building dependency tree Reading state information... Done Package libwebkitgtk-3.0-0 is not available, but is referred to by another package. This may mean that the package is missing, has been obsoleted, or is only available from another source
E: Package 'libwebkitgtk-3.0-0' has no installation candidate
Below the available webkit packages:
$ apt search libwebkit Sorting... Done Full Text Search... Done libwebkit2-sharp-4.0-cil/stable 2.10.9+git20160917-1.1 amd64 CLI bindings for WebKitGTK+ 4.0 using GObject Introspection libwebkit2-sharp-4.0-cil-dev/stable 2.10.9+git20160917-1.1 amd64 CLI bindings for WebKitGTK+ 4.0 using GObject Introspection - development libwebkit2gtk-4.0-37/stable,now 2.24.2-1 amd64 [installed,automatic] Web content engine library for GTK libwebkit2gtk-4.0-37-gtk2/stable 2.24.2-1 amd64 Web content engine library for GTK - GTK 2 plugin process libwebkit2gtk-4.0-dev/stable 2.24.2-1 amd64 Web content engine library for GTK - development files libwebkit2gtk-4.0-doc/stable 2.24.2-1 all Web content engine library for GTK - documentation