using IDE 10.1.1.606, can not exit program, pressing X or file>exit - nothing happens.
I have to exit with Windows task manager.
And - project does not remember the pins / clock setup I imported from files.
Please help...
I rechecked it, I can not exit IDE only after importing the pins file
Hello Ben,
are you using Pins and Clocks tools and importing settings from pin_mux.c?
Also, could you please attach the logs files located:
Regards,
Libor
Hello Ben,
the log does not show anything interesting, may be there's other file with previous log entries (.bak_0.log).
Anyway, I tried to reproduce it and it works fine for me (Win10) - click on exit asks me and then it asks me if I want to save the MEX configuration. May be if you open the Pins (active Pins perspective), do the import of settings from the C file and check, whether you have the save icon enabled:
If yes, please save it, so your work is not lost when killing the IDE.
You can just try to disable asking for closing the IDE in the preferences:
And last question - if you click on close the IDE - does the IDE works normally, or does it stop responding?
Regards,
Libor