RT1052 SDK 2.3.1 USB Middleware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1052 SDK 2.3.1 USB Middleware

1,186 Views
michaelwhite
Contributor II

Hello,

I recently upgraded the RT1052 SDK from 2.3.0 to 2.3.1 and now I no longer see USB middleware selection when I create a new project.  If I delete 2.3.1 and revert back to 2.3.0 I do see the USB middleware selection when I create a new project.  For now I've reverted back to 2.3.0.  Is there a reason the 2.3.1 USB middleware selection has disappeared?

Thanks.

0 Kudos
1 Reply

685 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Michael,

As the Note said in "5.1.1 SDK New Project Wizard: Basic Project Creation and Settings" of

"MCUXpresso_IDE_User_Guide.pdf"

Note: Some middleware components such as USB, are not currently compatible with the
New project wizard functionality and so will be hidden. The recommended approach if such
components are required is to import an example including the component and then modify this
as required. Please see SDK Project Component Management [53] for details of how this
might be done.

Hope it helps

TIC

0 Kudos