Hi there.
I am using a LPC54618J512-TFBGA180 and Pins Tool V3.
I created a new empty config and saved it as a *.mex file.
Only with processor and package setting,
nothing else defined.
Then I exported a pin list (html) from this *.mex file
and found pin D7 = VDD2
But according to data sheet
"LPC546xx - Rev. 1.8 - 14 June 2017" - p.50
this is VSS5 instead.
Also pin H5 = VSS6 is exported as VD1_00.
Where's the mistake, please ?
Hello,
Thanks for your sharing, this bug will be fixed on next release version MCUX_conf_tools_v_4.0_PRC2
Have a nice day!
Alice
Hello s. schott,
I haver reported it to MCUXpresso Configure tool expert team.
Sorry for the inconvenient to you.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------