Hello
Previously, I devellop project with codewarrior and KDS on K60/K70.
Today, I start a new project with K02 and then, Start with the new tools, Then MCUExpresso.
In it, I download the SDK for the K02, add some driver, middleware etc..
I configured my CPU, code "hello word" compile with some remark.
Many question:
1) The PRINTF("Hello word") is not recognized. Which component do I add to be taken?
2) I use the Spi, Then I Add the spi_adapter.
The DSPI_MasterInit is called from the generated file "Peripheral.c" => Ok
Now, I read the HAL dspi_adapter. If I want use it, there are a function HAL_SpiMasterInit which will call also DSPI_MasterInit… Then there is exemple code to use all the driver and HAL? with API detail, exemple code etc... I not find it!
3) The main function fall in infinite loop, then this is redundant with previous question, but I add timer / timer_manager. It seem with this I can configure and start some task. there is exemple? My need is to create some task, with different period and priority..
4) UART driver: how use the function LIN break detection? (may be response is in SDK documentation I asked in question 1?...)
Thank
解決済! 解決策の投稿を見る。
Hi,
Please check the following document and let me know if that is what you need.
https://community.nxp.com/docs/DOC-334074
Regards
Soledad
Ok
It is clear for me now.
I was confused with the printf via debug consol and a real UART.
Only what I need is via the console.
I will test that as soon as I will have the target!
Ok,
Then for the support of PrintF, can we modify an existing project to support it? If yes, how? I do not find how.
Hi,
You need to implement it by software, in the following link you will find more information about the lpuart driver
MCUXpresso SDK API Reference Manual: LPUART Driver
Regards
Soledad
Ok thank for the Lin.
What about add the printf on existing project?
Hi,
Please check the following document and let me know if that is what you need.
https://community.nxp.com/docs/DOC-334074
Regards
Soledad
Hi,
Did you create a new project? or Did you import a project?
Please check the following document and let me know if this helps with your questions:
https://community.nxp.com/docs/DOC-334074
Regarding the SPI example code, after download the sdk for k02, you can find the DSPI examples at the following path:
\SDK_2.7.0_MK02FN128xxx10.zip\boards\frdmk22f\driver_examples
In addition, I am attaching the MCUXpresso SDK API Reference Manual_MK22
Please let me know if this helps,
have a nice day!
Regards
Soledad
Hello
I start new project from scratch
-Which module exactly must I add to have the "PrintF" function?
-For the UART module, I think the C code is designed to configure the BreakLin Dtetection, but the MCU expresso IDE do not allow to activate this option. I'm right?
Alos, If I understand, If I use the UART_Adpater, I mudt not configure into MCUExpresso peripheral the UART? (Because It will init by the UART_adapter) I'm Right?
Hi,
Please follow the below steps:
1. Click on New project
2. Select the MCU from installed SDK, click Next
3. In project, Options select UART and add the uart driver
4. Select Redirect SDK "PRINTF" to C library "printf", then click Finish
5. At this point, you should be able to use printf.
Please check the fsl_uart.h
You will find the structure with the settings for all of the UART interrupt configurations.
I hope this helps, have a nice day !
Regards
Soledad
Hello,
Thank for the information about the Printf. But now, when the project is already existing, how set this functionnality?
For the LinBreak, it is what I said. The Break Lin interrupt detection is on the c code, but on the MCUXpresso, it is not ?
Hi,
MCUXpresso IDE does not allow to activate this option like you previously mentioned.
Regards
Soledad
Do you answer about the use of lin break or use of printf?
LinBreak