RT105x USB BC support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT105x USB BC support

1,654件の閲覧回数
mateuszpiesta
Contributor II

Hello,

We are designing custom device based on RT1051 uC which is battery powered. We need to have option for charging it trough USB Type-C connector. We are using external chip for Type-C support but we are also need to distinguish between dedicated/host chargers. We found that USB-PHY supports BC standard. Does NXP USB stack support BC ? 

There is USB_DEVICE_CHARGER_DETECT_ENABLE flag defined which suggests that such support is provided. After some digging in sources we also found that it needs FSL_FEATURE_SOC_USBDCD_COUNT set to compile. Unfortunately this flag is not defined in MIMXRT1051_features.h. Does that mean that RT1050 doesn't support BC or maybe USB stack is not yet prepared for BC support on RT1051 ?

Could you shed some light on this issue ?

Best regards

Mateusz Piesta

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,526件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Mateusz Piesta

or maybe USB stack is not yet prepared for BC support on RT1051 ?

USBDCD is not in RT1050, this is why the FSL_FEATURE_SOC_USBDCD_COUNT is cero, in the RT1050 devices you can find the USB_ANALOG in the USB-PHY part.

This Phy is capable of the charger detection which "detects whether the upstream-facing device is connected to a down-stream facing charger, either a dedicated USB charger or a host charger". Unfortunately, this is not implemented in the usb_phy.c file of the USB stack, so the customer would need to add it.

Hope this helps.

Best regards

0 件の賞賛
返信