Hello I am brand new to NXP devices (specifically the QN 9080 DK).
I am unable to run the basic wireless programs such as the examplified heart rate sensor FRTOS. I am able to Build, use Jlink debug probe, but my run terminates in error 127 (Still combing through documentation to find out what this means). If i could get some tips That would be great - my environment is the following: MacOS Catalina 10.15.5, Used Jlink driver install through LPCSrypt, and Jumpers @ JP16/15/8/7 (2-3)/12/13/14/11/2 (1-2). Red light on at D1, green light on at D4 and white LED on right next to D4/R48 (the RGB led) (no blinking they are just on). Also for the project I am just installing all of the drivers because I wanted to be sure that everything was being utilized in my MCUexpresso IDE project.
My ls /dev/tty.* output is:
/dev/tty.Bluetooth-Incoming-Port
/dev/tty.usbmodem0007217953211
I have the NXP IOT toolbox app on both android/iphone devices but both are unable to pick up the signal. Let me know what steps I may take, I tried an ISP reset, various configurations of jumpers, currently going to try it on my windows instead, thank you!
Hello!
I ended up figuring it out literaly 30 minutes after posting this, i just did a ISP reset before a regular reset call and that allowed my MCU expresso IDE debug probe to see the jLINK driver i installed via LPC scrypt.
Hi Eduardo,
It seems that you device entered into sleep mode.
By default, the example enables this mode. You can disable in the app_preinclude.c file
/* Use low power */
#define cPWR_UsePowerDownMode 0
Regards,
Mario
Hi, yes That is good to know! thank you!