MCUXpresso IDE (MacOs) Error reading from server (redlinkserv)
[Started server]
[Connected on port 3025]
redlink>ProbeList
Error reading from server (redlinkserv):
Read timed out
Hi,
I'm trying to debug the LPCX804 example code on the target. However, I'm having problems reaching the debug probe with MCUXpresso IDE on MacOS
I've tried:
Cannot write to server: not open (RedLinkServerException)
It has worked twice today. However, i most of the time I can't get any comms with the debug probe. to make this happen i've reconnected the USB and quickly sent the listProbes command:
Index = 1
Manufacturer = NXP Semiconductors
Description = LPC11U3x CMSIS-DAP v1.0.4
Serial Number = 0201000B
VID:PID = 1FC9:0132
Path = USB_1fc9_0132_14200000_ff00
I know the board works as i've tried it with a linux machine. However, i'd like to get it working on my personal laptop.
Many thanks,
Dan
Normally, you would only expect to see the probe come up in this mode if the reset button (S3) is held down as the board is powered up. So first of all check that the reset button isn't stuck down.
If that doesn't help ,then it sounds like you need to reprogram the probe firmware (though I can't think how you might have "lost" it).
The LPC11U3x based probe firmware can be found at: Firmware and drivers for LPC11U35 debug probes
There is also a link to this in the IDE's Help ->Additional Resources menu.
The user manual for the LPCXpresso804 contains information on how to program the firmware into the probe. You can download from:
but you may also find these articles of interest:
New debug probe firmware & drivers for MAX boards
Flashing and Installing the new firmware and drivers for LPC11U35 debug probes
Note you don't need to install drivers on macOS.
Anyway, please let us know if reprogramming the debug probe firmware helps resolve your issue.
Regards,
MCUXpresso IDE Support
You still haven't told us what version of mac OS you are running? I've just tried debugging an LPCXpresso804 board here on my Macbook Pro (15in, 2016 model) running macOS 10.14.6, and don't see any issues.
It would probably be worth trying the following, and see if anything helps:
Please also provide the output from running the following command in a terminal (when you have your LPCXpresso804 board attached to your Mac) :
system_profiler SPUSBDataType
Regards,
MCUXpresso IDE Support
Apologies,
macOS 10.14.5 (macbook Air, early 2014)
My board appears to still be in the firmware upgrade mode. I can't seem to connect it as a COM port:
sudo system_profiler SPUSBDataType
USB:
USB 3.0 Bus:
Host Controller Driver: AppleUSBXHCILPT
PCI Device ID: 0x9c31
PCI Revision ID: 0x0004
PCI Vendor ID: 0x8086
BRCM20702 Hub:
Product ID: 0x4500
Vendor ID: 0x0a5c (Broadcom Corp.)
Version: 1.00
Speed: Up to 12 Mb/sec
Manufacturer: Apple Inc.
Location ID: 0x14300000 / 3
Current Available (mA): 500
Current Required (mA): 94
Extra Operating Current (mA): 0
Built-In: Yes
Bluetooth USB Host Controller:
Product ID: 0x828f
Vendor ID: 0x05ac (Apple Inc.)
Version: 1.50
Speed: Up to 12 Mb/sec
Manufacturer: Apple Inc.
Location ID: 0x14330000 / 6
Current Available (mA): 500
Current Required (mA): 0
Extra Operating Current (mA): 0
Built-In: Yes
LPC1XXX IFLASH:
Product ID: 0x000f
Vendor ID: 0x1fc9 (NXP Semiconductors)
Version: 7.02
Serial Number: ISP
Speed: Up to 12 Mb/sec
Manufacturer: NXP
Location ID: 0x14100000 / 15
Current Available (mA): 500
Current Required (mA): 100
Extra Operating Current (mA): 0
We aren't seeing any issues debugging LPC804 board on macOS here. What version of macOS are you running?
But this sounds like something is stopping the low level debug server from starting up. Have you go any third party virus protection / firewall software running on your Mac?
Regards,
MCUXpresso IDE Support
thanks for your reply. I'm not running any anti virus. I've retried the above with the macOS firewall completely disabled. Same results. This may not be fixable :-(
Have you tried running as super user?
Same result when trying to debug a multi_timer_blinky project:
Read timed out
Read timed out
at com.crt.debugcommon.emulator.client.RedlinkServerClient.receive(RedlinkServerClient.java:945)
at com.crt.debugcommon.emulator.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1041)
at com.crt.debugcommon.emulator.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1022)
at com.crt.debugcommon.emulator.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1010)
at com.crt.debugcommon.emulator.client.RedlinkServerClient.probeList(RedlinkServerClient.java:917)
at com.crt.debugcommon.emulator.common.redlinkserver.RedlinkServerEmuHandler.discoverEmulators(RedlinkServerEmuHandler.java:200)
at com.crt.debugcommon.emulator.mac.AbstractMacServerProbe.discoverEmulators(AbstractMacServerProbe.java:78)
at com.crt.debugcommon.emulator.EmulatorsDB.getEmus(EmulatorsDB.java:338)
at com.crt.debugcommon.emulator.EmulatorsDB.getEmulatorInfo(EmulatorsDB.java:254)
at com.crt.debugcommon.emulator.EmulatorsDB.getAvailableEmulators(EmulatorsDB.java:182)
at com.crt.debugcommon.emulator.TargetDiscovery.getAvailableEmulators(TargetDiscovery.java:550)
at com.crt.debugcommon.emulator.CRTLaunchConfigHandler.probeDiscovery(CRTLaunchConfigHandler.java:831)
at com.crt.debugcommon.emulator.ProbeDiscoveryJob.run(ProbeDiscoveryJob.java:64)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:56)
[Started server]
[Connected on port 3025]
redlink>ProbeList
Error reading from server (redlinkserv):
Read timed out
No probes found
[Closed]
[Started server]
[Connected on port 3025]
redlink>ProbeList
Error reading from server (redlinkserv):
Read timed out
Hello Dan,
I recommend you to update the firmware and drivers of LPC11U35. Please check the below document for instructions.
Flashing and Installing the new firmware and drivers for LPC11U35 debug probes
Hope it helps!
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks for you reply Felipe. I'm running macOS, not windows. I tried the firmware upgrade but now the board keeps mounting as CRP DISABLED when i power it on. What should i do?