I am using KL25Z micro controller along with FRDM33771BSPIEVB Evaluation board.When I am trying to build my source code (main .c file) in the MCUXpresso IDE platform and I am getting the following message "**** Build of configuration FLASH for project BCCEvaluationSW **** Nothing to build for project BCCEvaluationSW"
Hi Thiruvonasundari,
As I see, I think you're using the MC33771 / MC33772 (Battery Cell Controller) Demo and Driver Library, this library is for Code Warrior 10.6 or higher. I would suggest to download the last Code Warrior version (v11.1).
I hope this helps you.
Best Regards,
Alexis Andalon
Hi Alexis I installed Code Warrior 11.1. I tried with "hello world "example it was building but when I am trying to build my source file nothing happened. When I open Properties-> Tool chain editor it shows
"Orphaned configuration. No base extension cfg exists for org.eclipse.cdt.cross.arm.gnu.sourcery.windows.elf.debug.2136167795".
"Orphaned toolchain org.eclipse.cdt.cross.arm.gnu.sourcery.windows.elf.toolchain.debug.777954515 (ARM Ltd Windows GCC (G++ Lite))".
Thanks
Hi Thiruvonasundari,
I'll explain how to import an example to code warrior.
Please click in the next option to import the project to your workspace:
After that, select the folder in which your project is located, the next option will appear in the window, select the project and the option to copy the project in to the workspace:
After this, you would need to make a clean in the project, for this please click in the next option:
After this, if you build your project you shouldn't have any error.
I hope this helps you.
Best Regards,
Alexis Andalon
Thanks Alex it works!
Best regards
Sundari
Looks like you have created your own build configuration called "FLASH". I would compare the settings for that build config with one of the standard configs (Debug and Release) and see what is different.