Hi, I'm using the i.MX1060 EVK board and MCUExpresso.
I'm working on a hardware design that can't be simulated well on desktop, so I have to do a lot of compile/flash cycles to test on the evaluation board directly.
So currently, after making any change, I have to:
There has to be a faster way! Can you help me understand how to flash in one button or keyboard shortcut?
In addition to the fully feature functionality of the GUI Flash Tool (which will always trigger a probe discovery), you can also use the "Program Flash action ..." option on the Debug shortcuts in the Quickstart Panel, as described in section 12.3.1, "Debug Quickstart Shortcuts". For further details also see 12.3.6, "Project Flash Programming" in the MCUXpresso IDE v11.0 User Guide.
Alternatively, you can just launch a debug session - which will generally trigger and build then launch a debug session (including automatically programming flash as the debug session starts).
Regards,
MCUXpresso IDE Support