Do the LPCXpresso work with ULINK2 debugger tool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do the LPCXpresso work with ULINK2 debugger tool?

1,894 Views
waynekim
Contributor I

Now i am going to use LPC11E67JBM100. so i have checked web site. it's OK LPCXpresso tool.

then i have an ULINK2 . the question is the Ulink2  can be worked with LPCXpresso?

thanks!

0 Kudos
Reply
2 Replies

1,355 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Wayne,

Yes, CMSIS-DAP probes such as Keil uLINK with CMSIS-DAP firmware are supported. I would recommend that you consider using the newer MCUXpresso IDE product (which has superseded the older LPCXpresso IDE product). 

For more details and to download, please visit : http://www.nxp.com/mcuxpresso/ide


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

1,355 Views
waynekim
Contributor I

Hi!

Thank you for reply!

It’s helpful to me.

BRs

Wayne

0 Kudos
Reply