Hi,
I have an LPCXpresso LPC11U24 dev board which I can't get MCUXpresso to connect to.
I have previously had the board working on a different PC running LPCXpresso.
I am running on fresh install of Ubuntu Linux, a fresh MCUXpresso install 10.0.2_411 and a supported development board plugged directly into the PC.
The system recognises the board:
$ lsusb
Bus 001 Device 016: ID 0471:df55 Philips (or NXP) LPCXpresso LPC-Link
I can connect to it using dfu-util:
$ dfu-util -l
dfu-util 0.9Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/Deducing device DFU version from functional descriptor length
Found Runtime: [0471:df55] ver=0001, devnum=16, cfg=1, intf=0, path="1-2", alt=0, name="UNKNOWN", serial="UNKNOWN"
I can configure the device using boot_link1
$ ./boot_link1
Looking for DFU devices with VID 0471 PID df55 ...
dfu-util -d 0471:df55 -c 1 -i 0 -t 2048 -R -D /usr/local/mcuxpressoide-10.0.2_411/ide/bin/LPCXpressoWIN.enc
Booted LPC-Link (0471:df55) with /usr/local/mcuxpressoide-10.0.2_411/ide/bin/LPCXpressoWIN.enc$ lsusb
Bus 001 Device 017: ID 1fc9:0009 NXP Semiconductors
I cannot, despite considerable fiddling get it recognised by the RedlinkServer
redlink>ProbeList
No probes found
Any suggestions for how I can connect to the board?
David
I adjusted and restarted my networking and rebooted a few times and it has now mysteriously connected for the first time.
NFI why, will update if I can figure it out.