Build a project with mcu MKL17Z64VFM4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build a project with mcu MKL17Z64VFM4

Jump to solution
829 Views
wen-fang_pan
Contributor I

Now I use MCU MKL17Z64VFM4 to create a new project:

1. Use online MCUXpresso SDK Builder to select mcu MKL17Z64xxx4/use pin toll config pin/use clock tool config clock, named the sdk as SDK_2.6.0_MKL17Z64xxx4 then Build MCUXpresso SDK, Down the SDK as three folders,SDK_2.6.0_MKL17Z64xxx4.zip/SDK_2.6.0_MKL17Z64xxx4_doc.zip/SDK_2.6.0_MKL17Z64xxx4_ConfigTools_data

pastedImage_1.png

2. Add the sdk SDK_2.6.0_mkl17z64xxx4.zip to MCUXpresso IDE.

3.In MCUXpresso IDE-QuickStart select "Import SDK example(s)" I can not select MKL17Z64xxx4 but only can select MKL27Z64xxx4 to create a project. The project use mcu MKL27Z64xxx4, if I want to use MKL17Z64xxx4 only to change the mcu? The sdk can only created by mcu which have a board,It is too strange, I never got those trouble when I use other mcus.

0 Kudos
Reply
1 Solution
753 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Wenfang,

KL17 hasn't FRDM or TWR board. So, in it's SDK there isn't MCUXpresso demo. KL17 is a KL27 without USB. You can use KL27 demo to test. When you will create a KL17 project in MCUXpresso, the only way is QuickStart panel->New project.

Regards,

Jing

View solution in original post

0 Kudos
Reply
2 Replies
753 Views
wen-fang_pan
Contributor I

Hi Jing:

   Ihave already creat new KL17Z64VFM4 project: Qickstart Create or Import a project->New Project.

It seems that every mcu must create a SDK using SDK builder before create a project.

    I use KL17Z64VFM4 project within MCUXpresso IDE. When I use the config tools in the MCUXpresso IDE to config the project , there is a warning like below:

   工具链(IDT)工程中,该版本的GPIO Driver不被支持,所需的:2.2.1,实际的:2.3.2

   but the compile and build is OK, is there any hidden danger about this?

0 Kudos
Reply
754 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Wenfang,

KL17 hasn't FRDM or TWR board. So, in it's SDK there isn't MCUXpresso demo. KL17 is a KL27 without USB. You can use KL27 demo to test. When you will create a KL17 project in MCUXpresso, the only way is QuickStart panel->New project.

Regards,

Jing

0 Kudos
Reply